Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DraftBodyBuilder.MatchingScope |
DraftBodyBuilder.MatchingScope.ALL
All faces-to-draft are to be matched
|
static DraftBodyBuilder.MatchingScope |
DraftBodyBuilder.MatchingScope.ALL_BUT_SELECTED
All faces-to-draft except the ones explicitly indicated are to be matched
|
Modifier and Type | Method and Description |
---|---|
DraftBodyBuilder.MatchingScope |
DraftBodyBuilder.matchScope()
Returns the match scope
License requirements: None. |
static DraftBodyBuilder.MatchingScope |
DraftBodyBuilder.MatchingScope.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBodyBuilder.MatchingScope |
DraftBodyBuilder.MatchingScope.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBodyBuilder.MatchingScope[] |
DraftBodyBuilder.MatchingScope.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DraftBodyBuilder.setMatchScope(DraftBodyBuilder.MatchingScope matchingScope)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.