Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DraftBodyBuilder.MatchOption |
DraftBodyBuilder.MatchOption.ALL
All faces-to-draft are to be matched
|
static DraftBodyBuilder.MatchOption |
DraftBodyBuilder.MatchOption.ALL_BUT_SELECTED
All faces-to-draft except the ones explicitly indicated are to be matched
|
static DraftBodyBuilder.MatchOption |
DraftBodyBuilder.MatchOption.NONE
No match option is specified
|
Modifier and Type | Method and Description |
---|---|
DraftBodyBuilder.MatchOption |
DraftBodyBuilder.matchingOption()
Deprecated.
Deprecated in NX9.0.0. Use
DraftBodyBuilder.matchScope() instead
|
static DraftBodyBuilder.MatchOption |
DraftBodyBuilder.MatchOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBodyBuilder.MatchOption |
DraftBodyBuilder.MatchOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBodyBuilder.MatchOption[] |
DraftBodyBuilder.MatchOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DraftBodyBuilder.setMatchingOption(DraftBodyBuilder.MatchOption matchingOption)
Deprecated.
Deprecated in NX9.0.0. Use
DraftBodyBuilder.setMatchScope(nxopen.features.DraftBodyBuilder.MatchingScope) instead
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.