Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DivideCurveBuilder.KnotPointOption |
DivideCurveBuilder.KnotPointOption.ALL_KNOTPOINTS
All Knotpoints
|
static DivideCurveBuilder.KnotPointOption |
DivideCurveBuilder.KnotPointOption.BY_NUMBER
By Number
|
static DivideCurveBuilder.KnotPointOption |
DivideCurveBuilder.KnotPointOption.SELECT_POINT
Screen Position
|
Modifier and Type | Method and Description |
---|---|
DivideCurveBuilder.KnotPointOption |
DivideCurveBuilder.knotPointMethod()
Returns the knot point method
License requirements: None. |
static DivideCurveBuilder.KnotPointOption |
DivideCurveBuilder.KnotPointOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DivideCurveBuilder.KnotPointOption |
DivideCurveBuilder.KnotPointOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DivideCurveBuilder.KnotPointOption[] |
DivideCurveBuilder.KnotPointOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DivideCurveBuilder.setKnotPointMethod(DivideCurveBuilder.KnotPointOption knotPointMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.