Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DivideCurveBuilder.CornerOption |
DivideCurveBuilder.CornerOption.ALL_CORNERPOINTS
All Cornerpoints
|
static DivideCurveBuilder.CornerOption |
DivideCurveBuilder.CornerOption.BY_NUMBER
By Number
|
static DivideCurveBuilder.CornerOption |
DivideCurveBuilder.CornerOption.SELECT_POINT
Screen Position
|
Modifier and Type | Method and Description |
---|---|
DivideCurveBuilder.CornerOption |
DivideCurveBuilder.cornerMethod()
Returns the corner method
License requirements: None. |
static DivideCurveBuilder.CornerOption |
DivideCurveBuilder.CornerOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DivideCurveBuilder.CornerOption |
DivideCurveBuilder.CornerOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DivideCurveBuilder.CornerOption[] |
DivideCurveBuilder.CornerOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DivideCurveBuilder.setCornerMethod(DivideCurveBuilder.CornerOption cornerMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.