Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.CURVE_OR_FACE_AXIS
Datum axis at the curve or face axis
|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.FIXED
Indicate the datum axis is fixed
|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.INFERRED
Inferred
|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.INTERSECTION
Datum axis at the intersection of objects
|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.ON_CURVE_VECTOR
Datum axis at vector on curve
|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.POINT_AND_DIR
Datum axis thru a point and parallel or perpendicular to direction
|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.TWO_POINTS
Datum axis thru two point
|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.XC_AXIS
Datum axis thru X axis
|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.YC_AXIS
Datum axis thru Y axis
|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.ZC_AXIS
Datum axis thru Z axis
|
Modifier and Type | Method and Description |
---|---|
DatumAxisBuilder.Types |
DatumAxisBuilder.type()
Returns the Datum Axis type
License requirements: None. |
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumAxisBuilder.Types |
DatumAxisBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumAxisBuilder.Types[] |
DatumAxisBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumAxisBuilder.setType(DatumAxisBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.