Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DatumAxisBuilder.FixedType |
DatumAxisBuilder.FixedType.ALL
Fixed datum axis thru all Axis
|
static DatumAxisBuilder.FixedType |
DatumAxisBuilder.FixedType.X
Fixed datum axis thru X Axis
|
static DatumAxisBuilder.FixedType |
DatumAxisBuilder.FixedType.Y
Fixed datum axis thru Y Axis
|
static DatumAxisBuilder.FixedType |
DatumAxisBuilder.FixedType.Z
Fixed datum axis thru Z Axis
|
Modifier and Type | Method and Description |
---|---|
static DatumAxisBuilder.FixedType |
DatumAxisBuilder.FixedType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumAxisBuilder.FixedType |
DatumAxisBuilder.FixedType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumAxisBuilder.FixedType[] |
DatumAxisBuilder.FixedType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumAxisBuilder.setFixedDatumAxis(DatumAxisBuilder.FixedType type)
Sets type of fixed datum axis
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.