Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DatumAxisBuilder.CurveOrientations |
DatumAxisBuilder.CurveOrientations.BINORMAL
Orientation at binormal to curve
|
static DatumAxisBuilder.CurveOrientations |
DatumAxisBuilder.CurveOrientations.NORMAL
Orientation at normal to curve
|
static DatumAxisBuilder.CurveOrientations |
DatumAxisBuilder.CurveOrientations.PARALLEL_TO_OBJECT
Orientation at parallel to object
|
static DatumAxisBuilder.CurveOrientations |
DatumAxisBuilder.CurveOrientations.PERPENDICULAR_TO_OBJECT
Orientation at perpendicular to object
|
static DatumAxisBuilder.CurveOrientations |
DatumAxisBuilder.CurveOrientations.TANGENT
Orientation at tangent to curve
|
Modifier and Type | Method and Description |
---|---|
DatumAxisBuilder.CurveOrientations |
DatumAxisBuilder.curveOrientation()
Returns the orientation of vector on a curve.
|
static DatumAxisBuilder.CurveOrientations |
DatumAxisBuilder.CurveOrientations.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumAxisBuilder.CurveOrientations |
DatumAxisBuilder.CurveOrientations.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumAxisBuilder.CurveOrientations[] |
DatumAxisBuilder.CurveOrientations.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumAxisBuilder.setCurveOrientation(DatumAxisBuilder.CurveOrientations curveOrientation)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.