Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.ANGLE
Angle constraint
|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.CENTER
Center constraint
|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.COINCIDENT
Coincident constraint
|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.DISTANCE
Distance constraint
|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.FRENET
Frenet constraint
|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.PARALLEL
Parallel constraint
|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.PERPENDICULAR
Perpendicular constraint
|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.TANGENT
Tangent constraint
|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.UNDEFINED
Not defined
|
Modifier and Type | Method and Description |
---|---|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumAxisBuilder.ConstraintType |
DatumAxisBuilder.ConstraintType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumAxisBuilder.ConstraintType[] |
DatumAxisBuilder.ConstraintType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumAxisBuilder.setGeometryAndConstraints(DisplayableObject geometry1,
DatumAxisBuilder.ConstraintType geometryConstraintType1,
int constraintAttribute1,
double constraintValue1,
String constraint1,
DisplayableObject geometry2,
DatumAxisBuilder.ConstraintType geometryConstraintType2,
int constraintAttribute2,
double constraintValue2,
String constraint2,
Sense direction)
Sets two different geometric objects.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.