Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static CylinderBuilder.Types |
CylinderBuilder.Types.ARC_AND_HEIGHT
Arc and Height
|
static CylinderBuilder.Types |
CylinderBuilder.Types.AXIS_DIAMETER_AND_HEIGHT
Axis, Diameter and Height
|
Modifier and Type | Method and Description |
---|---|
CylinderBuilder.Types |
CylinderBuilder.type()
Returns the type
License requirements: None. |
static CylinderBuilder.Types |
CylinderBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CylinderBuilder.Types |
CylinderBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CylinderBuilder.Types[] |
CylinderBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CylinderBuilder.setType(CylinderBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.