Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
CustomAttribute.Type[] |
CustomFeatureData.AllCustomAttributeNameAndTypesData.attributetype |
static CustomAttribute.Type |
CustomAttribute.Type.BOOL
Bool.
|
static CustomAttribute.Type |
CustomAttribute.Type.BOOL_VLA
Bool variable length array.
|
static CustomAttribute.Type |
CustomAttribute.Type.DOUBLE
Double.
|
static CustomAttribute.Type |
CustomAttribute.Type.DOUBLE_VLA
Double variable length array.
|
static CustomAttribute.Type |
CustomAttribute.Type.EXPRESSION
Expression.
|
static CustomAttribute.Type |
CustomAttribute.Type.EXPRESSION_VLA
Expression variable length array.
|
static CustomAttribute.Type |
CustomAttribute.Type.INTEGER
Integer.
|
static CustomAttribute.Type |
CustomAttribute.Type.INTEGER_VLA
Integer variable length array.
|
static CustomAttribute.Type |
CustomAttribute.Type.STRING
String.
|
static CustomAttribute.Type |
CustomAttribute.Type.STRING_VLA
String variable length array.
|
static CustomAttribute.Type |
CustomAttribute.Type.TAG
Reference.
|
static CustomAttribute.Type |
CustomAttribute.Type.TAG_VLA
Reference variable length array.
|
static CustomAttribute.Type |
CustomAttribute.Type.UNKNOWN
Invalid or unknown.
|
Modifier and Type | Method and Description |
---|---|
CustomAttribute.Type |
CustomAttribute.typeValue()
Returns the custom attribute type value
License requirements: solid_modeling ("SOLIDS MODELING") . |
static CustomAttribute.Type |
CustomAttribute.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomAttribute.Type |
CustomAttribute.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomAttribute.Type[] |
CustomAttribute.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
boolean |
CustomFeatureData.hasCustomAttribute(String attributeName,
CustomAttribute.Type type)
Checks if the custom feature attribute of given name and type exists
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.