Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static CustomAttribute.Property |
CustomAttribute.Property.IS_OUTPUT_ATTRIBUTE
Output Attribute
|
static CustomAttribute.Property |
CustomAttribute.Property.IS_OWNED_ATTRIBUTE
Owned Attribute
|
static CustomAttribute.Property |
CustomAttribute.Property.IS_REFERENCING_TARGET_BODY
Attribute Referencing to target body
|
static CustomAttribute.Property |
CustomAttribute.Property.MANDATORY_INPUT |
Modifier and Type | Method and Description |
---|---|
CustomAttribute.Property[] |
CustomAttribute.getProperties()
The custom attribute get all properties
License requirements: solid_modeling ("SOLIDS MODELING") . |
static CustomAttribute.Property |
CustomAttribute.Property.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomAttribute.Property |
CustomAttribute.Property.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomAttribute.Property[] |
CustomAttribute.Property.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CustomAttribute.addProperty(CustomAttribute.Property attributeProperty)
The custom attribute add property
License requirements: solid_modeling ("SOLIDS MODELING") . |
CustomDoubleArrayAttribute |
CustomAttributeCollection.createCustomDoubleArrayAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomDoubleArrayAttribute with parameters. |
CustomDoubleAttribute |
CustomAttributeCollection.createCustomDoubleAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomDoubleAttribute with parameters. |
CustomExpressionArrayAttribute |
CustomAttributeCollection.createCustomExpressionArrayAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomExpressionArrayAttribute with parameters. |
CustomExpressionAttribute |
CustomAttributeCollection.createCustomExpressionAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomExpressionAttribute with parameters. |
CustomIntegerArrayAttribute |
CustomAttributeCollection.createCustomIntegerArrayAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomIntegerArrayAttribute with parameters. |
CustomIntegerAttribute |
CustomAttributeCollection.createCustomIntegerAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomIntegerAttribute with parameters. |
CustomLogicalArrayAttribute |
CustomAttributeCollection.createCustomLogicalArrayAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomLogicalArrayAttribute with parameters. |
CustomLogicalAttribute |
CustomAttributeCollection.createCustomLogicalAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomLogicalAttribute with parameters. |
CustomStringArrayAttribute |
CustomAttributeCollection.createCustomStringArrayAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomStringArrayAttribute with parameters. |
CustomStringAttribute |
CustomAttributeCollection.createCustomStringAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomStringAttribute with parameters. |
CustomTagArrayAttribute |
CustomAttributeCollection.createCustomTagArrayAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomTagArrayAttribute with parameters. |
CustomTagAttribute |
CustomAttributeCollection.createCustomTagAttribute(String attributeName,
CustomAttribute.Property[] attributeProperties)
Creates an
CustomTagAttribute with parameters. |
boolean |
CustomAttribute.hasProperty(CustomAttribute.Property attributeProperty)
The custom attribute does property exist on attribute
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
CustomAttribute.removeProperty(CustomAttribute.Property attributeProperty)
The custom attribute remove property
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.