Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AddendumSection
Represents an Addendum Section feature
To create or edit an instance of this class, use AddendumSectionBuilder Created in NX7.5.0 |
interface |
BridgeCurve
Represents a bridge curve feature
To create or edit an instance of this class, use BridgeCurveBuilderEx Created in NX5.0.0 |
interface |
GeodesicChamfer
Represents a GeodesicChamfer feature.
|
interface |
GeodesicFillet
Represents a GeodesicFillet feature.
|
interface |
GeodesicIntersect
Represents a GeodesicIntersect feature.
|
interface |
GeodesicLine
Represents a GeodesicLine feature.
|
interface |
GeodesicOffset
Represents a GeodesicOffset feature.
|
interface |
GeodesicPoint
Represents a GeodesicPoint feature.
|
interface |
GeodesicProject
Represents a GeodesicProject feature.
|
interface |
GeodesicSketch
Represents a GeodesicSketch feature.
|
interface |
GeodesicTrim
Represents a GeodesicTrim feature.
|
interface |
IntersectionCurve
Represents a
IntersectionCurve . |
interface |
IsoclineCurve
Represents a isocline curve feature
To create or edit an instance of this class, use IsoclineCurveBuilder Created in NX11.0.0 |
interface |
IsoparametricCurves
Represents a isoparametric curves feature
To create or edit an instance of this class, use IsoparametricCurvesBuilder Created in NX8.0.0 |
interface |
Offset3DCurve
Represents a offset 3D curve feature
To create or edit an instance of this class, use Offset3DCurveBuilder Created in NX10.0.0 |
interface |
OffsetCurve
Represents a offset curve feature
To create or edit an instance of this class, use OffsetCurveBuilder Created in NX5.0.0 |
interface |
PointSet
Represents a point set feature
To create or edit an instance of this class, use PointSetBuilder Created in NX6.0.0 |
interface |
ProjectCurve
Represents a project curve feature.
|
interface |
ScaleCurve
Represents a scale curve feature
To create or edit an instance of this class, use ScaleCurveBuilder Created in NX11.0.0 |
interface |
ServiceOrientedFeatureCurve
Represents a curve feature
To create or edit an instance of this class, use ServiceOrientedFeatureCurveBuilder Created in NX11.0.0 |
interface |
SmoothSpline
Represents a smooth spline feature
To create or edit an instance of this class, use SmoothSplineBuilder Created in NX6.0.0 |
interface |
SpineCurve
Represents a spine curve feature
To create or edit an instance of this class, use SpineCurveBuilder Created in NX11.0.0 |
interface |
TrimCurve
Represents a trim curve feature
To create or edit an instance of this class, use TrimCurveBuilder Created in NX5.0.0 |
interface |
TrimCurve2
Represents a new trim curve feature feature
To create or edit an instance of this class, use TrimCurve2Builder Created in NX11.0.1 |
interface |
VirtualCurve
Represents a virtual curve feature
To create or edit an instance of this class, use VirtualCurveBuilder Created in NX7.5.0 |
interface |
WrapUnwrap
Represents a wrap or unwrap curve feature
To create or edit an instance of this class, use WrapBuilder Created in NX6.0.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
EdgeReinforcement
Represents a edge reinforcement feature.
|
interface |
ExpansionDrawing
Represents a expansion drawing feature.
|
interface |
InverseBendingLines
Represents a inverse bending lines feature
To create or edit an instance of this class, use InverseBendingLinesBuilder Created in NX8.0.0 |
interface |
ManufacturingPreparation
Represents a manufacturing preparation feature
To create or edit an instance of this class, use ManufacturingPreparationBuilder Created in NX8.0.2 |
interface |
PillarSystem
Represents a pillar system feature.
|
interface |
ProfileSystem
Represents a profile system feature.
|
interface |
ReferenceLine
Represents a reference line feature.
|
interface |
RollingLine
Represents a rolling line feature.
|
interface |
Seam
Represents a ship design seam feature.
|
interface |
StandardPart
Represents a standard part feature.
|
interface |
StiffenerSystem
Represents a stiffener system feature.
|
interface |
TraceLines
Represents a trace lines feature
To create or edit an instance of this class, use TraceLinesBuilder Created in NX7.5.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
HoodVisibility
Represents a hood visibility spline feature
To create or edit an instance of this class, use HoodVisibilityBuilder Created in NX6.0.0 |
interface |
ReflectionData
Represents a reflection data feature
To create or edit an instance of this class, use ReflectionDataBuilder Created in NX6.0.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
SurfaceWeld
Represents a surface weld feature
To create or edit an instance of this class, use SurfaceWeldBuilder Created in NX9.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.