Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static CopyPasteBuilder.BuilderVersion |
CopyPasteBuilder.BuilderVersion.EXPOSE_BODY
Value of version which exposes additional target body parent; It should be added since NX8.5.
|
static CopyPasteBuilder.BuilderVersion |
CopyPasteBuilder.BuilderVersion.EXPOSE_ONFLY_SO
Value of version which exposes smart object created on fly as part of the copy operation; It should be set since NX8.0.
|
static CopyPasteBuilder.BuilderVersion |
CopyPasteBuilder.BuilderVersion.ORIGINAL
Value of original version; It can be set before NX8.0.
|
static CopyPasteBuilder.BuilderVersion |
CopyPasteBuilder.BuilderVersion.SHOW_PARENT_SELECT_OPTION
Value of version which introduces parent select option; It should be added since NX8.5.1.
|
Modifier and Type | Method and Description |
---|---|
CopyPasteBuilder.BuilderVersion |
CopyPasteBuilder.getBuilderVersion()
The builder version getting function
License requirements: solid_modeling ("SOLIDS MODELING") . |
static CopyPasteBuilder.BuilderVersion |
CopyPasteBuilder.BuilderVersion.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CopyPasteBuilder.BuilderVersion |
CopyPasteBuilder.BuilderVersion.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CopyPasteBuilder.BuilderVersion[] |
CopyPasteBuilder.BuilderVersion.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CopyPasteBuilder.setBuilderVersion(CopyPasteBuilder.BuilderVersion version)
The builder version setting function.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.