Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ConeBuilder.Types |
ConeBuilder.Types.BASE_DIAMETER_HEIGHT_AND_HALF_ANGLE
Represents type of cone created by providing Base Diameter, Height and Half Angle
|
static ConeBuilder.Types |
ConeBuilder.Types.DIAMETERS_AND_HALF_ANGLE
Represents type of cone created by providing Diameters and Half Angle
|
static ConeBuilder.Types |
ConeBuilder.Types.DIAMETERS_AND_HEIGHT
Represents type of cone created by providing Diameters and Height
|
static ConeBuilder.Types |
ConeBuilder.Types.TOP_DIAMETER_HEIGHT_AND_HALF_ANGLE
Represents type of cone created by providing Top Diameter, Height and Half Angle
|
static ConeBuilder.Types |
ConeBuilder.Types.TWO_COAXIAL_ARCS
Represents type of cone created by providing Two Coaxial Arcs
|
Modifier and Type | Method and Description |
---|---|
ConeBuilder.Types |
ConeBuilder.type()
Returns the type represented by
ConeBuilder.Types
License requirements: None. |
static ConeBuilder.Types |
ConeBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConeBuilder.Types |
ConeBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConeBuilder.Types[] |
ConeBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ConeBuilder.setType(ConeBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.