Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BooleanFeature
Represents a boolean feature.
|
interface |
BridgeTransition
Represents a bridge transition feature
To create or edit an instance of this class, use BridgeTransitionBuilder Created in NX5.0.2 |
interface |
EmbossBody
Represents an emboss body feature
To create or edit an instance of this class, use EmbossBodyBuilder Created in NX8.5.0 |
interface |
PasteFace
Represents a paste face feature
To create or edit an instance of this class, use PasteFaceBuilder Created in NX6.0.0 |
interface |
Patch
Represents a Patch feature
To create or edit an instance of this class, use PatchBuilder Created in NX6.0.1 |
interface |
Sew
Represents a sew feature.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.