Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ColorFeatureBuilder.OperationType |
ColorFeatureBuilder.OperationType.NO_COLOR
remove color from feature
|
static ColorFeatureBuilder.OperationType |
ColorFeatureBuilder.OperationType.SPECIFY_COLOR
assign color to feature
|
Modifier and Type | Method and Description |
---|---|
ColorFeatureBuilder.OperationType |
ColorFeatureBuilder.specifyColor()
Returns the specified color option.
|
static ColorFeatureBuilder.OperationType |
ColorFeatureBuilder.OperationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ColorFeatureBuilder.OperationType |
ColorFeatureBuilder.OperationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ColorFeatureBuilder.OperationType[] |
ColorFeatureBuilder.OperationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ColorFeatureBuilder.setSpecifyColor(ColorFeatureBuilder.OperationType specifyColor)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.