Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static CircularBlendCurveBuilder.CylinderDirectionOption |
CircularBlendCurveBuilder.CylinderDirectionOption.BEST_FIT
Best fit method
|
static CircularBlendCurveBuilder.CylinderDirectionOption |
CircularBlendCurveBuilder.CylinderDirectionOption.CURRENT_VIEW
Current view method
|
static CircularBlendCurveBuilder.CylinderDirectionOption |
CircularBlendCurveBuilder.CylinderDirectionOption.VARIABLE
Variable method
|
static CircularBlendCurveBuilder.CylinderDirectionOption |
CircularBlendCurveBuilder.CylinderDirectionOption.VECTOR
Specify vector method
|
Modifier and Type | Method and Description |
---|---|
CircularBlendCurveBuilder.CylinderDirectionOption |
CircularBlendCurveBuilder.directionOption()
Returns the cylinder direction option as
CircularBlendCurveBuilder.CylinderDirectionOption
License requirements: None. |
static CircularBlendCurveBuilder.CylinderDirectionOption |
CircularBlendCurveBuilder.CylinderDirectionOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CircularBlendCurveBuilder.CylinderDirectionOption |
CircularBlendCurveBuilder.CylinderDirectionOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CircularBlendCurveBuilder.CylinderDirectionOption[] |
CircularBlendCurveBuilder.CylinderDirectionOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CircularBlendCurveBuilder.setDirectionOption(CircularBlendCurveBuilder.CylinderDirectionOption directionOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.