Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ChamferBuilder.ChamferOption |
ChamferBuilder.ChamferOption.OFFSET_AND_ANGLE
Offset distance and angle
|
static ChamferBuilder.ChamferOption |
ChamferBuilder.ChamferOption.SYMMETRIC_OFFSETS
Symmetric offsets
|
static ChamferBuilder.ChamferOption |
ChamferBuilder.ChamferOption.TWO_OFFSETS
Two offset distances
|
Modifier and Type | Method and Description |
---|---|
ChamferBuilder.ChamferOption |
ChamferBuilder.option()
Returns the chamfer parameter option.
|
static ChamferBuilder.ChamferOption |
ChamferBuilder.ChamferOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ChamferBuilder.ChamferOption |
ChamferBuilder.ChamferOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ChamferBuilder.ChamferOption[] |
ChamferBuilder.ChamferOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ChamferBuilder.setOption(ChamferBuilder.ChamferOption opt)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.