Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilderEx.StartObjectTypes |
BridgeCurveBuilderEx.StartObjectTypes.OBJECT
A point or face
|
static BridgeCurveBuilderEx.StartObjectTypes |
BridgeCurveBuilderEx.StartObjectTypes.SECTION
Section
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilderEx.StartObjectTypes |
BridgeCurveBuilderEx.startObjectType()
Returns the start object type
License requirements: None. |
static BridgeCurveBuilderEx.StartObjectTypes |
BridgeCurveBuilderEx.StartObjectTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilderEx.StartObjectTypes |
BridgeCurveBuilderEx.StartObjectTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilderEx.StartObjectTypes[] |
BridgeCurveBuilderEx.StartObjectTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilderEx.setStartObjectType(BridgeCurveBuilderEx.StartObjectTypes startObjectType)
License requirements: solid_modeling ("SOLIDS MODELING") OR nx_freeform_1 ("basic freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.