Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilderEx.RadiusConstraintMethods |
BridgeCurveBuilderEx.RadiusConstraintMethods.MINIMUM
Minimum radius
|
static BridgeCurveBuilderEx.RadiusConstraintMethods |
BridgeCurveBuilderEx.RadiusConstraintMethods.NONE
No constraint
|
static BridgeCurveBuilderEx.RadiusConstraintMethods |
BridgeCurveBuilderEx.RadiusConstraintMethods.PEAK
Peak radius
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilderEx.RadiusConstraintMethods |
BridgeCurveBuilderEx.radiusConstraintMethod()
Returns the radius constraint method
License requirements: None. |
static BridgeCurveBuilderEx.RadiusConstraintMethods |
BridgeCurveBuilderEx.RadiusConstraintMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilderEx.RadiusConstraintMethods |
BridgeCurveBuilderEx.RadiusConstraintMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilderEx.RadiusConstraintMethods[] |
BridgeCurveBuilderEx.RadiusConstraintMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilderEx.setRadiusConstraintMethod(BridgeCurveBuilderEx.RadiusConstraintMethods radiusConstraintMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR nx_freeform_1 ("basic freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.