Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilderEx.EndObjectTypes |
BridgeCurveBuilderEx.EndObjectTypes.DATUM
A datum plane or axis for symmetric constraint
|
static BridgeCurveBuilderEx.EndObjectTypes |
BridgeCurveBuilderEx.EndObjectTypes.OBJECT
A point or face
|
static BridgeCurveBuilderEx.EndObjectTypes |
BridgeCurveBuilderEx.EndObjectTypes.SECTION
Section
|
static BridgeCurveBuilderEx.EndObjectTypes |
BridgeCurveBuilderEx.EndObjectTypes.VECTOR
A vector representing a plane for symmetric constraint
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilderEx.EndObjectTypes |
BridgeCurveBuilderEx.endObjectType()
Returns the end object type
License requirements: None. |
static BridgeCurveBuilderEx.EndObjectTypes |
BridgeCurveBuilderEx.EndObjectTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilderEx.EndObjectTypes |
BridgeCurveBuilderEx.EndObjectTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilderEx.EndObjectTypes[] |
BridgeCurveBuilderEx.EndObjectTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilderEx.setEndObjectType(BridgeCurveBuilderEx.EndObjectTypes endObjectType)
License requirements: solid_modeling ("SOLIDS MODELING") OR nx_freeform_1 ("basic freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.