Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilder.SurfaceDirectionTypes |
BridgeCurveBuilder.SurfaceDirectionTypes.ISO_U
bridge direction takes u-isoparametric direction
of the base surface at the selected point
|
static BridgeCurveBuilder.SurfaceDirectionTypes |
BridgeCurveBuilder.SurfaceDirectionTypes.ISO_V
bridge direction takes v-isoparametric direction
of the base surface at the selected point
|
static BridgeCurveBuilder.SurfaceDirectionTypes |
BridgeCurveBuilder.SurfaceDirectionTypes.SECTIONAL
bridge direction takes non-isoparametric direction
of the base surface at the selected point
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilder.SurfaceDirectionTypes |
BridgeCurveBuilder.endSurfaceDirectionOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
BridgeCurveBuilder.SurfaceDirectionTypes |
BridgeCurveBuilder.startSurfaceDirectionOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
static BridgeCurveBuilder.SurfaceDirectionTypes |
BridgeCurveBuilder.SurfaceDirectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.SurfaceDirectionTypes |
BridgeCurveBuilder.SurfaceDirectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.SurfaceDirectionTypes[] |
BridgeCurveBuilder.SurfaceDirectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilder.setEndSurfaceDirectionOption(BridgeCurveBuilder.SurfaceDirectionTypes endSurfaceDirectionOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
void |
BridgeCurveBuilder.setStartSurfaceDirectionOption(BridgeCurveBuilder.SurfaceDirectionTypes startSurfaceDirectionOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.