Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilder.ShapeControlTypes |
BridgeCurveBuilder.ShapeControlTypes.CONIC
conic parameter
|
static BridgeCurveBuilder.ShapeControlTypes |
BridgeCurveBuilder.ShapeControlTypes.END_POINT
end point conditions
|
static BridgeCurveBuilder.ShapeControlTypes |
BridgeCurveBuilder.ShapeControlTypes.PEAK_POINT
peak point conditions
|
static BridgeCurveBuilder.ShapeControlTypes |
BridgeCurveBuilder.ShapeControlTypes.SHAPE_CURVE
shape curve
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilder.ShapeControlTypes |
BridgeCurveBuilder.shapeControlOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
static BridgeCurveBuilder.ShapeControlTypes |
BridgeCurveBuilder.ShapeControlTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.ShapeControlTypes |
BridgeCurveBuilder.ShapeControlTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.ShapeControlTypes[] |
BridgeCurveBuilder.ShapeControlTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilder.setShapeControlOption(BridgeCurveBuilder.ShapeControlTypes shapeControlOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.