Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilder.MinRadiusTypes |
BridgeCurveBuilder.MinRadiusTypes.MINIMUM
regular
|
static BridgeCurveBuilder.MinRadiusTypes |
BridgeCurveBuilder.MinRadiusTypes.NONE
no minimum radius
|
static BridgeCurveBuilder.MinRadiusTypes |
BridgeCurveBuilder.MinRadiusTypes.PEAK
peak
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilder.MinRadiusTypes |
BridgeCurveBuilder.minimumRadiusOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
static BridgeCurveBuilder.MinRadiusTypes |
BridgeCurveBuilder.MinRadiusTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.MinRadiusTypes |
BridgeCurveBuilder.MinRadiusTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.MinRadiusTypes[] |
BridgeCurveBuilder.MinRadiusTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilder.setMinimumRadiusOption(BridgeCurveBuilder.MinRadiusTypes minimumRadiusOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.