Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilder.CurveDirectionTypes |
BridgeCurveBuilder.CurveDirectionTypes.PERPENDICULAR
bridge direction takes the direction that is
perpendicular to the tangent direction
of the base curve at the selected point
|
static BridgeCurveBuilder.CurveDirectionTypes |
BridgeCurveBuilder.CurveDirectionTypes.TANGENT
bridge direction takes the tangent direction
of the base curve at the selected point
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilder.CurveDirectionTypes |
BridgeCurveBuilder.endCurveDirectionOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
BridgeCurveBuilder.CurveDirectionTypes |
BridgeCurveBuilder.startCurveDirectionOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
static BridgeCurveBuilder.CurveDirectionTypes |
BridgeCurveBuilder.CurveDirectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.CurveDirectionTypes |
BridgeCurveBuilder.CurveDirectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.CurveDirectionTypes[] |
BridgeCurveBuilder.CurveDirectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilder.setEndCurveDirectionOption(BridgeCurveBuilder.CurveDirectionTypes endCurveDirectionOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
void |
BridgeCurveBuilder.setStartCurveDirectionOption(BridgeCurveBuilder.CurveDirectionTypes startCurveDirectionOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.