Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilder.ConstraintTypes |
BridgeCurveBuilder.ConstraintTypes.G0
G0 continuity
|
static BridgeCurveBuilder.ConstraintTypes |
BridgeCurveBuilder.ConstraintTypes.G1
G1 continuity
|
static BridgeCurveBuilder.ConstraintTypes |
BridgeCurveBuilder.ConstraintTypes.G2
G2 continuity
|
static BridgeCurveBuilder.ConstraintTypes |
BridgeCurveBuilder.ConstraintTypes.G3
G3 continuity
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilder.ConstraintTypes |
BridgeCurveBuilder.endContinuityOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
BridgeCurveBuilder.ConstraintTypes |
BridgeCurveBuilder.startContinuityOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
static BridgeCurveBuilder.ConstraintTypes |
BridgeCurveBuilder.ConstraintTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.ConstraintTypes |
BridgeCurveBuilder.ConstraintTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.ConstraintTypes[] |
BridgeCurveBuilder.ConstraintTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilder.setEndContinuityOption(BridgeCurveBuilder.ConstraintTypes endContinuityOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
void |
BridgeCurveBuilder.setStartContinuityOption(BridgeCurveBuilder.ConstraintTypes startContinuityOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.