Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BodyByEquationBuilder.StlFileUnitTypes |
BodyByEquationBuilder.StlFileUnitTypes.INCHES
STL unit is inches.
|
static BodyByEquationBuilder.StlFileUnitTypes |
BodyByEquationBuilder.StlFileUnitTypes.METERS
STL unit is meters.
|
static BodyByEquationBuilder.StlFileUnitTypes |
BodyByEquationBuilder.StlFileUnitTypes.MILLIMETERS
STL unit is millimeters.
|
Modifier and Type | Method and Description |
---|---|
BodyByEquationBuilder.StlFileUnitTypes |
BodyByEquationBuilder.stlFileUnits()
Returns the option to specify the size of an STL unit.
|
static BodyByEquationBuilder.StlFileUnitTypes |
BodyByEquationBuilder.StlFileUnitTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BodyByEquationBuilder.StlFileUnitTypes |
BodyByEquationBuilder.StlFileUnitTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BodyByEquationBuilder.StlFileUnitTypes[] |
BodyByEquationBuilder.StlFileUnitTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BodyByEquationBuilder.setStlFileUnits(BodyByEquationBuilder.StlFileUnitTypes stlFileUnits)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.