Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BlendCornerBuilder.ContinuityTypes |
BlendCornerBuilder.ContinuityTypes.G1
Tangent continuity
|
static BlendCornerBuilder.ContinuityTypes |
BlendCornerBuilder.ContinuityTypes.G2
Curvature continuity
|
Modifier and Type | Method and Description |
---|---|
BlendCornerBuilder.ContinuityTypes |
BlendCornerBuilder.continuity()
Returns the continuity type
License requirements: None. |
static BlendCornerBuilder.ContinuityTypes |
BlendCornerBuilder.ContinuityTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BlendCornerBuilder.ContinuityTypes |
BlendCornerBuilder.ContinuityTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BlendCornerBuilder.ContinuityTypes[] |
BlendCornerBuilder.ContinuityTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BlendCornerBuilder.setContinuity(BlendCornerBuilder.ContinuityTypes continuity)
License requirements: nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.