Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.StartOption.ALONG_XC
Along XC
|
static AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.StartOption.ALONG_YC
Along YC
|
static AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.StartOption.ALONG_ZC
Along ZC
|
static AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.StartOption.AT_ANGLE
At angle
|
static AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.StartOption.INFERRED
Inferred
|
static AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.StartOption.NORMAL
Normal
|
static AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.StartOption.POINT
Point
|
static AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.StartOption.TANGENT
Tangent
|
Modifier and Type | Method and Description |
---|---|
AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.startPointOptions()
Returns the start point options
License requirements: None. |
static AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.StartOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssociativeLineBuilder.StartOption |
AssociativeLineBuilder.StartOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssociativeLineBuilder.StartOption[] |
AssociativeLineBuilder.StartOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssociativeLineBuilder.setStartPointOptions(AssociativeLineBuilder.StartOption startPointOptions)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.