Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AssociativeArcBuilder.StartReference |
AssociativeArcBuilder.StartReference.ABSOLUTE
Absolute CSYS
|
static AssociativeArcBuilder.StartReference |
AssociativeArcBuilder.StartReference.CORDINATES_SYSTEM
CSYS
|
static AssociativeArcBuilder.StartReference |
AssociativeArcBuilder.StartReference.WCS
WCS
|
Modifier and Type | Method and Description |
---|---|
AssociativeArcBuilder.StartReference |
AssociativeArcBuilder.startPointReference()
Returns the start point reference
License requirements: None. |
static AssociativeArcBuilder.StartReference |
AssociativeArcBuilder.StartReference.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssociativeArcBuilder.StartReference |
AssociativeArcBuilder.StartReference.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssociativeArcBuilder.StartReference[] |
AssociativeArcBuilder.StartReference.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssociativeArcBuilder.setStartPointReference(AssociativeArcBuilder.StartReference startPointReference)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.