Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AestheticFaceBlendBuilder.ShapeType |
AestheticFaceBlendBuilder.ShapeType.ACCELERATED
Accelerated option will generate more shapes depending on the size of the center radius and continuity specified.
|
static AestheticFaceBlendBuilder.ShapeType |
AestheticFaceBlendBuilder.ShapeType.CIRCULAR
Circular option will always generate a constant radius arc shape.
|
Modifier and Type | Method and Description |
---|---|
AestheticFaceBlendBuilder.ShapeType |
AestheticFaceBlendBuilder.shapeOption()
Deprecated.
Deprecated in NX8.0.0. Use
AestheticFaceBlendBuilder.isAccelerated() instead.
|
static AestheticFaceBlendBuilder.ShapeType |
AestheticFaceBlendBuilder.ShapeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AestheticFaceBlendBuilder.ShapeType |
AestheticFaceBlendBuilder.ShapeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AestheticFaceBlendBuilder.ShapeType[] |
AestheticFaceBlendBuilder.ShapeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AestheticFaceBlendBuilder.setShapeOption(AestheticFaceBlendBuilder.ShapeType shapeOption)
Deprecated.
Deprecated in NX8.0.0. Use
AestheticFaceBlendBuilder.setAccelerated(boolean) instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.