Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AeroFlangeBuilder.ThicknessDimensionOptions |
AeroFlangeBuilder.ThicknessDimensionOptions.SIMPLE |
static AeroFlangeBuilder.ThicknessDimensionOptions |
AeroFlangeBuilder.ThicknessDimensionOptions.SYMMETRIC |
Modifier and Type | Method and Description |
---|---|
AeroFlangeBuilder.ThicknessDimensionOptions |
AeroFlangeBuilder.thicknessDimensionType()
Returns the thickness dimension type
License requirements: None. |
static AeroFlangeBuilder.ThicknessDimensionOptions |
AeroFlangeBuilder.ThicknessDimensionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AeroFlangeBuilder.ThicknessDimensionOptions |
AeroFlangeBuilder.ThicknessDimensionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AeroFlangeBuilder.ThicknessDimensionOptions[] |
AeroFlangeBuilder.ThicknessDimensionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AeroFlangeBuilder.setThicknessDimensionType(AeroFlangeBuilder.ThicknessDimensionOptions thicknessDimensionType)
License requirements: nx_aero_design (" NX Aero Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.