Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AdmMoveFaceBuilder.MoveOptionType |
AdmMoveFaceBuilder.MoveOptionType.CUT_AND_PASTE
Option equates to enhanced Move Face with Cut or Copy Face with Paste Face and Delete Face without heal.
|
static AdmMoveFaceBuilder.MoveOptionType |
AdmMoveFaceBuilder.MoveOptionType.MOVE_AND_ADAPT
Option equates to standard Move Face.
|
Modifier and Type | Method and Description |
---|---|
AdmMoveFaceBuilder.MoveOptionType |
AdmMoveFaceBuilder.moveOption()
Returns the move option.
|
static AdmMoveFaceBuilder.MoveOptionType |
AdmMoveFaceBuilder.MoveOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AdmMoveFaceBuilder.MoveOptionType |
AdmMoveFaceBuilder.MoveOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AdmMoveFaceBuilder.MoveOptionType[] |
AdmMoveFaceBuilder.MoveOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AdmMoveFaceBuilder.setMoveOption(AdmMoveFaceBuilder.MoveOptionType moveOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.