Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AOCSBuilder.CurveOffsetTypes |
AOCSBuilder.CurveOffsetTypes.THROUGH_POINT
Through Point
|
static AOCSBuilder.CurveOffsetTypes |
AOCSBuilder.CurveOffsetTypes.VALUE
Value
|
Modifier and Type | Method and Description |
---|---|
AOCSBuilder.CurveOffsetTypes |
AOCSBuilder.curveOffsetType()
Returns the curve offset type
License requirements: solid_modeling ("SOLIDS MODELING") OR insp_programming ("INSPECTION PROGRAMMING") . |
static AOCSBuilder.CurveOffsetTypes |
AOCSBuilder.CurveOffsetTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AOCSBuilder.CurveOffsetTypes |
AOCSBuilder.CurveOffsetTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AOCSBuilder.CurveOffsetTypes[] |
AOCSBuilder.CurveOffsetTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AOCSBuilder.setCurveOffsetType(AOCSBuilder.CurveOffsetTypes type)
Sets the curve offset type
License requirements: solid_modeling ("SOLIDS MODELING") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.