public interface WrapGeometryBuilder extends FeatureBuilder
WrapGeometry
builder
FeatureCollection.createWrapGeometryBuilder(nxopen.features.WrapGeometry)
Property | Value |
---|---|
AddOffset.Value | 0 (millimeters part), 0 (inches part) |
Associative | 1 |
CloseGaps | Sharp |
DistTol | 2.54 |
IsInterpart | 0 |
SplitOffset.Value | 0 (millimeters part), 0 (inches part) |
Modifier and Type | Interface and Description |
---|---|
static class |
WrapGeometryBuilder.CloseGapType
Represents the close gap type
|
Modifier and Type | Method and Description |
---|---|
Expression |
addOffset()
Returns the Additional offset.
|
boolean |
associative()
Returns the Remove parms switch
License requirements: None. |
WrapGeometryBuilder.CloseGapType |
closeGaps()
Returns the Method used to close the gaps after offset of the wrap
License requirements: None. |
double |
distTol()
Returns the Distance tolerance used to facet the solids.
|
SelectDisplayableObjectList |
geometry()
Returns the geometry to be wrapped (solid, sheet, curve, point)
License requirements: None. |
boolean |
isInterpart()
Returns the Setting that determines if this feature have interpart references
License requirements: None. |
PlaneList |
planesList()
Returns the Planes to split the geometry, tightens the wrap along this plane
License requirements: None. |
void |
setAssociative(boolean associative)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setCloseGaps(WrapGeometryBuilder.CloseGapType closeGaps)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setDistTol(double distTol)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setInterpart(boolean isInterpart)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Expression |
splitOffset()
Returns the Offset applied to both sides of the splitting planes.
|
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectDisplayableObjectList geometry() throws NXException, RemoteException
NXException
RemoteException
PlaneList planesList() throws NXException, RemoteException
NXException
RemoteException
boolean associative() throws NXException, RemoteException
NXException
RemoteException
void setAssociative(boolean associative) throws NXException, RemoteException
associative
- NXException
RemoteException
WrapGeometryBuilder.CloseGapType closeGaps() throws NXException, RemoteException
NXException
RemoteException
void setCloseGaps(WrapGeometryBuilder.CloseGapType closeGaps) throws NXException, RemoteException
closeGaps
- NXException
RemoteException
Expression addOffset() throws NXException, RemoteException
NXException
RemoteException
Expression splitOffset() throws NXException, RemoteException
NXException
RemoteException
double distTol() throws NXException, RemoteException
NXException
RemoteException
void setDistTol(double distTol) throws NXException, RemoteException
distTol
- NXException
RemoteException
boolean isInterpart() throws NXException, RemoteException
NXException
RemoteException
void setInterpart(boolean isInterpart) throws NXException, RemoteException
isInterpart
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.