public interface ChangeShellThicknessBuilder extends FeatureBuilder
ChangeShellThickness
builder FeatureCollection.createChangeShellThicknessBuilder(nxopen.features.ChangeShellThickness)
Property | Value |
---|---|
FacesToChangeThickness.CoaxialEnabled | 0 |
FacesToChangeThickness.CoplanarAxesEnabled | 0 |
FacesToChangeThickness.CoplanarEnabled | 0 |
FacesToChangeThickness.EqualDiameterEnabled | 0 |
FacesToChangeThickness.OffsetEnabled | 0 |
FacesToChangeThickness.ParallelEnabled | 0 |
FacesToChangeThickness.PerpendicularEnabled | 0 |
FacesToChangeThickness.SymmetricEnabled | 0 |
FacesToChangeThickness.TangentEnabled | 0 |
FacesToChangeThickness.ThicknessChainEnabled | 0 |
FacesToChangeThickness.UseFaceBrowse | 1 |
NeighborsEnabled | True |
WallThickness.Value | 5.0 (millimeters part), 0.5 (inches part) |
Modifier and Type | Method and Description |
---|---|
void |
addEntities(NXObject[] entities)
Adds entities which have same wall thickness value as the selected face
License requirements: None. |
FaceRecognitionBuilder |
facesToChangeThickness()
Returns the faces to be selected to change thickness
License requirements: None. |
boolean |
neighborsEnabled()
Returns the flag to select neighbor faces that have the same wall thickness value as the face selected.
|
void |
removeEntities(NXObject[] entities)
Removes entities
License requirements: None. |
void |
setNeighborsEnabled(boolean selectNeighbors)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Expression |
wallThickness()
Returns the wall thickness
License requirements: None. |
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
FaceRecognitionBuilder facesToChangeThickness() throws NXException, RemoteException
NXException
RemoteException
boolean neighborsEnabled() throws NXException, RemoteException
NXException
RemoteException
void setNeighborsEnabled(boolean selectNeighbors) throws NXException, RemoteException
selectNeighbors
- NXException
RemoteException
Expression wallThickness() throws NXException, RemoteException
NXException
RemoteException
void addEntities(NXObject[] entities) throws NXException, RemoteException
entities
- Objects to addNXException
RemoteException
void removeEntities(NXObject[] entities) throws NXException, RemoteException
entities
- Objects to removeNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.