Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static SectionViewBuilder.SectionLineType |
SectionViewBuilder.SectionLineType.HALF |
static SectionViewBuilder.SectionLineType |
SectionViewBuilder.SectionLineType.POINT_AND_ANGLE |
static SectionViewBuilder.SectionLineType |
SectionViewBuilder.SectionLineType.POINT_TO_POINT |
static SectionViewBuilder.SectionLineType |
SectionViewBuilder.SectionLineType.REVOLVED |
static SectionViewBuilder.SectionLineType |
SectionViewBuilder.SectionLineType.SIMPLE_STEPPED |
Modifier and Type | Method and Description |
---|---|
SectionViewBuilder.SectionLineType |
SectionViewBuilder.sectionViewType()
Returns the section line type
License requirements: None. |
static SectionViewBuilder.SectionLineType |
SectionViewBuilder.SectionLineType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionViewBuilder.SectionLineType |
SectionViewBuilder.SectionLineType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionViewBuilder.SectionLineType[] |
SectionViewBuilder.SectionLineType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionViewBuilder.setSectionViewType(SectionViewBuilder.SectionLineType sectionLineType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.