public static class SectionViewBuilder.SectionLineType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HALF |
static int |
_POINT_AND_ANGLE |
static int |
_POINT_TO_POINT |
static int |
_REVOLVED |
static int |
_SIMPLE_STEPPED |
static SectionViewBuilder.SectionLineType |
HALF |
static SectionViewBuilder.SectionLineType |
POINT_AND_ANGLE |
static SectionViewBuilder.SectionLineType |
POINT_TO_POINT |
static SectionViewBuilder.SectionLineType |
REVOLVED |
static SectionViewBuilder.SectionLineType |
SIMPLE_STEPPED |
Modifier and Type | Method and Description |
---|---|
static SectionViewBuilder.SectionLineType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionViewBuilder.SectionLineType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionViewBuilder.SectionLineType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SectionViewBuilder.SectionLineType SIMPLE_STEPPED
public static final SectionViewBuilder.SectionLineType HALF
public static final SectionViewBuilder.SectionLineType REVOLVED
public static final SectionViewBuilder.SectionLineType POINT_TO_POINT
public static final SectionViewBuilder.SectionLineType POINT_AND_ANGLE
public static final int _SIMPLE_STEPPED
public static final int _HALF
public static final int _REVOLVED
public static final int _POINT_TO_POINT
public static final int _POINT_AND_ANGLE
public static SectionViewBuilder.SectionLineType valueOf(int value)
public static SectionViewBuilder.SectionLineType valueOf(String name)
public static SectionViewBuilder.SectionLineType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.