Package | Description |
---|---|
nxopen.drafting |
Provides classes and interfaces for the Drafting.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Method and Description |
---|---|
EditSectionLineSettingsBuilder |
SettingsManager.createDrawingEditSectionLineSettingsBuilder(SectionLine[] sectionLines)
Creates a
EditSectionLineSettingsBuilder
For multiple object settings, first create primary settings builder by passing all selected 'n' objects.Then create 'n-1' secondary builders by passing single selected object starting from second selected object. |
Modifier and Type | Interface and Description |
---|---|
interface |
BaseHalfSectionLine
Represents a Base Half Section Line.
|
interface |
BasePointToPointSectionLine
Represents a Base Point to Point Section Line.
|
interface |
BaseSteppedSectionLine
Represents a Base Stepped Section Line.
|
interface |
HalfPictorialSectionLine
Half Pictorial Section Line is used to create a pictorial view with
half of the part sectioned and the other half un-sectioned.
|
interface |
HalfSectionLine
Half Section Line is used to create a view with half of the part
sectioned and the other half un-sectioned.
|
interface |
OrientedSectionLine
Represents a Oriented Section Line.
|
interface |
PictorialSectionLine
A Pictorial Simple or Pictorial Stepped Section Line.
|
interface |
PointAndAngleSectionLine
Point and Angle Section Line lets you create a view with multiple
segment cuts with no bends.
|
interface |
PointToPointSectionLine
Point to Point Section Line lets you create a view with multiple
segment cuts with no bends.
|
interface |
RevolvedSectionLine
Revolved Section Line is used to create section views which are
revolved about an axis.
|
interface |
SketchedHalfSectionLine
Sketched Half Section Line is sketch based section line.
|
interface |
SketchedPointToPointSectionLine
Sketched Point to Point Section Line is sketch based section line.
|
interface |
SketchedSteppedSectionLine
A Sketched Simple or Stepped Section Line is sketch based section line.
|
interface |
SteppedSectionLine
A Simple or Stepped Section Line.
|
Modifier and Type | Field and Description |
---|---|
SectionLine |
SelectSectionLine.ValueData.selection
selected object
|
SectionLine |
SelectSectionLine.ValueWithCaeSetObjectInfoData.selection
selected object
|
SectionLine |
SelectSectionLine.ValueWithSnapData.selection1
first selected object
|
SectionLine |
SelectSectionLine.ValueWithSnapData.selection2
second selected object
|
Modifier and Type | Method and Description |
---|---|
SectionLine |
SelectSectionLine.value()
Returns the object being selected
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SectionLineBuilder |
SectionLineCollection.createSectionLineBuilder(SectionLine sectionLine)
Deprecated.
Deprecated in NX10.0.0. Use
SectionViewBuilder.sectionLineSegments() instead.
|
SectionLineStyleBuilder |
SectionLineCollection.createSectionLineStyleBuilder(SectionLine sectionline)
Deprecated.
Deprecated in NX10.0.0. Use
ViewSectionLineBuilder instead.
|
SketchSectionLineBuilder |
SectionLineCollection.createSketchSectionLineBuilder(SectionLine sectionLine)
Creates the Sketch Section Line builder
License requirements: drafting ("DRAFTING") . |
void |
SectionLineSettingsBuilder.inheritSettingsFromSelectedObjects(SectionLine selectedObject)
Inherit Settings From Selected Objects
License requirements: drafting ("DRAFTING") . |
void |
EditSectionLineSettingsBuilder.inheritSettingsFromSelectedObjects(SectionLine selectedObject)
Inherit Settings From Selected Objects
License requirements: drafting ("DRAFTING") . |
void |
SelectSectionLine.setValue(SectionLine selection)
Sets the object being selected
License requirements: None. |
void |
SelectSectionLine.setValue(SectionLine selection,
View view,
Point3d point)
The object being selected with the object's view and object's point
License requirements: None. |
void |
SelectSectionLine.setValueWithCaeSetObjectInfo(SectionLine selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObject.setValue(nxopen.TaggedObject) .
|
void |
SelectSectionLine.setValueWithSnap(InferSnapType.SnapType snapType,
SectionLine selection1,
View view1,
Point3d point1,
SectionLine selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.