Interface | Description |
---|---|
AnnotateViewsBuilder |
This class is used to annotate views based on the knowledge fusion rules.
|
AttributeItemBuilder |
Represents a
AttributeItemBuilder . |
AttributeItemBuilderList |
Represents a list of objects.
|
AutomationManager |
Represents a
AutomationManager . |
AutomationPreferencesBuilder |
the builder for Drafting Automation Preferences
To create a new instance of this class, use AutomationManager.createPreferencesBuilder() Created in NX8.0.0 |
AutomationRuleBuilder | |
BaseEditSettingsBuilder |
Represents a
BaseEditSettingsBuilder . |
CutCopyPasteBuilder |
Represents a paste in Drafting.
|
CutCopyPasteLeaderBuilder |
Represents a Drafting Paste, especially when reassociating a leader on paste.
|
DistributeAnnotationsBuilder |
This class is used to distribute annotations associated to a view.
|
DraftingApplicationManager |
Represents an object that manages drafting objects and member views.
|
DrawingAutomationWizard |
Represents callback data for the drawing automation wizard.
|
DrawingCreationWizardBuilder |
Represents a
DrawingCreationWizardBuilder . |
MoveToDrawingViewBuilder |
This builder allows the user to extract contents from a sheet and transfer them to a new Drawing
view, also provide some other options for view creation
To create a new instance of this class, use DraftingApplicationManager.createMoveToDrawingViewBuilder() Default values. |
PreferencesBuilder |
Represents a
PreferencesBuilder builder To create a new instance of this class, use SettingsManager.createPreferencesBuilder() Default values. |
PrimaryContentItemBuilder |
Represents a
PrimaryContentItemBuilder . |
PrimaryContentItemBuilderList |
Represents a list of objects.
|
RulesBuilder |
This class is used to specify knowledge fusion rules in a drawing template.
|
SettingsManager |
Represents an object that manages drafting settings.
|
SmashDrawingViewBuilder |
This builder allows the user to break a Drawing View into its parts and delete the Drawing View
To create a new instance of this class, use DraftingApplicationManager.createSmashDrawingViewBuilder() Created in NX8.5.0 |
SpecifyRuleBuilder |
This class is used to specify knowledge fusion rule for a note object in a drawing template.
|
Class | Description |
---|---|
AnnotateViewsBuilder.ExistingAutomaticAnnotation |
Option to delete or preserve existing automatic annotations when annotation views command
is run.
|
AutomationManager.RemainingPartsOfBookletData |
This class holds the data returned from
AutomationManager.getRemainingPartsOfBooklet() |
CutCopyPasteBuilder.TypeOperation |
Specifies the copy cut operation type.
|
CutCopyPasteBuilder.TypePaste |
Specifies the paste type.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.