Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static CustomViewSettingsBuilder.ThreadStandards |
CustomViewSettingsBuilder.ThreadStandards.ANSI_DETAILED |
static CustomViewSettingsBuilder.ThreadStandards |
CustomViewSettingsBuilder.ThreadStandards.ANSI_SCHEMATIC |
static CustomViewSettingsBuilder.ThreadStandards |
CustomViewSettingsBuilder.ThreadStandards.ANSI_SIMPLIFIED |
static CustomViewSettingsBuilder.ThreadStandards |
CustomViewSettingsBuilder.ThreadStandards.ESKD_SIMPLIFIED |
static CustomViewSettingsBuilder.ThreadStandards |
CustomViewSettingsBuilder.ThreadStandards.ISO_DETAILED |
static CustomViewSettingsBuilder.ThreadStandards |
CustomViewSettingsBuilder.ThreadStandards.ISO_SIMPLIFIED |
static CustomViewSettingsBuilder.ThreadStandards |
CustomViewSettingsBuilder.ThreadStandards.NONE |
Modifier and Type | Method and Description |
---|---|
CustomViewSettingsBuilder.ThreadStandards |
CustomViewSettingsBuilder.threadStandard()
Returns the thread standard
License requirements: None. |
static CustomViewSettingsBuilder.ThreadStandards |
CustomViewSettingsBuilder.ThreadStandards.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomViewSettingsBuilder.ThreadStandards |
CustomViewSettingsBuilder.ThreadStandards.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomViewSettingsBuilder.ThreadStandards[] |
CustomViewSettingsBuilder.ThreadStandards.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CustomViewSettingsBuilder.setThreadStandard(CustomViewSettingsBuilder.ThreadStandards threadStandard)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.