public static class CustomViewSettingsBuilder.ThreadStandards extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANSI_DETAILED |
static int |
_ANSI_SCHEMATIC |
static int |
_ANSI_SIMPLIFIED |
static int |
_ESKD_SIMPLIFIED |
static int |
_ISO_DETAILED |
static int |
_ISO_SIMPLIFIED |
static int |
_NONE |
static CustomViewSettingsBuilder.ThreadStandards |
ANSI_DETAILED |
static CustomViewSettingsBuilder.ThreadStandards |
ANSI_SCHEMATIC |
static CustomViewSettingsBuilder.ThreadStandards |
ANSI_SIMPLIFIED |
static CustomViewSettingsBuilder.ThreadStandards |
ESKD_SIMPLIFIED |
static CustomViewSettingsBuilder.ThreadStandards |
ISO_DETAILED |
static CustomViewSettingsBuilder.ThreadStandards |
ISO_SIMPLIFIED |
static CustomViewSettingsBuilder.ThreadStandards |
NONE |
Modifier and Type | Method and Description |
---|---|
static CustomViewSettingsBuilder.ThreadStandards |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomViewSettingsBuilder.ThreadStandards |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomViewSettingsBuilder.ThreadStandards[] |
values()
Returns an array that contains the values for this enum.
|
public static final CustomViewSettingsBuilder.ThreadStandards NONE
public static final CustomViewSettingsBuilder.ThreadStandards ANSI_SIMPLIFIED
public static final CustomViewSettingsBuilder.ThreadStandards ANSI_SCHEMATIC
public static final CustomViewSettingsBuilder.ThreadStandards ANSI_DETAILED
public static final CustomViewSettingsBuilder.ThreadStandards ISO_SIMPLIFIED
public static final CustomViewSettingsBuilder.ThreadStandards ISO_DETAILED
public static final CustomViewSettingsBuilder.ThreadStandards ESKD_SIMPLIFIED
public static final int _NONE
public static final int _ANSI_SIMPLIFIED
public static final int _ANSI_SCHEMATIC
public static final int _ANSI_DETAILED
public static final int _ISO_SIMPLIFIED
public static final int _ISO_DETAILED
public static final int _ESKD_SIMPLIFIED
public static CustomViewSettingsBuilder.ThreadStandards valueOf(int value)
public static CustomViewSettingsBuilder.ThreadStandards valueOf(String name)
public static CustomViewSettingsBuilder.ThreadStandards[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.