Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static CustomViewSettingsBuilder.Interfering |
CustomViewSettingsBuilder.Interfering.NONE |
static CustomViewSettingsBuilder.Interfering |
CustomViewSettingsBuilder.Interfering.WITH_INTERFERENCE |
static CustomViewSettingsBuilder.Interfering |
CustomViewSettingsBuilder.Interfering.WITHOUT_INTERFERENCE |
Modifier and Type | Method and Description |
---|---|
CustomViewSettingsBuilder.Interfering |
CustomViewSettingsBuilder.interferingSolids()
Returns the interfering solids
License requirements: None. |
static CustomViewSettingsBuilder.Interfering |
CustomViewSettingsBuilder.Interfering.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomViewSettingsBuilder.Interfering |
CustomViewSettingsBuilder.Interfering.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomViewSettingsBuilder.Interfering[] |
CustomViewSettingsBuilder.Interfering.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CustomViewSettingsBuilder.setInterferingSolids(CustomViewSettingsBuilder.Interfering interferingSolids)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.