public static class CustomViewSettingsBuilder.Interfering extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE |
static int |
_WITH_INTERFERENCE |
static int |
_WITHOUT_INTERFERENCE |
static CustomViewSettingsBuilder.Interfering |
NONE |
static CustomViewSettingsBuilder.Interfering |
WITH_INTERFERENCE |
static CustomViewSettingsBuilder.Interfering |
WITHOUT_INTERFERENCE |
Modifier and Type | Method and Description |
---|---|
static CustomViewSettingsBuilder.Interfering |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomViewSettingsBuilder.Interfering |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomViewSettingsBuilder.Interfering[] |
values()
Returns an array that contains the values for this enum.
|
public static final CustomViewSettingsBuilder.Interfering NONE
public static final CustomViewSettingsBuilder.Interfering WITHOUT_INTERFERENCE
public static final CustomViewSettingsBuilder.Interfering WITH_INTERFERENCE
public static final int _NONE
public static final int _WITHOUT_INTERFERENCE
public static final int _WITH_INTERFERENCE
public static CustomViewSettingsBuilder.Interfering valueOf(int value)
public static CustomViewSettingsBuilder.Interfering valueOf(String name)
public static CustomViewSettingsBuilder.Interfering[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.