Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static Wall.MaterialTextureType |
Wall.MaterialTextureType.IMAGE_FILE
The wall uses image for tiling.
|
static Wall.MaterialTextureType |
Wall.MaterialTextureType.INVISIBLE
The wall is not displayed.
|
static Wall.MaterialTextureType |
Wall.MaterialTextureType.SHADOW_CATCHER
The wall is transparent, and is used to display
shadows.
|
Modifier and Type | Method and Description |
---|---|
static Wall.MaterialTextureType |
Wall.MaterialTextureType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Wall.MaterialTextureType |
Wall.MaterialTextureType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Wall.MaterialTextureType[] |
Wall.MaterialTextureType.values()
Returns an array that contains the values for this enum.
|
Wall.MaterialTextureType |
Wall.wallMaterialTextureType()
Returns the wall material texture type - either shadow_catcher, image file, or invisible
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
Wall.setWallMaterialTextureType(Wall.MaterialTextureType wallMaterialType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.