Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static TrueShadingBuilder.SurfaceOrientType |
TrueShadingBuilder.SurfaceOrientType.BACK
Project shadows onto the back wall
|
static TrueShadingBuilder.SurfaceOrientType |
TrueShadingBuilder.SurfaceOrientType.BOTTOM
Project shadows onto the floor
|
static TrueShadingBuilder.SurfaceOrientType |
TrueShadingBuilder.SurfaceOrientType.BOTTOM_FIXED
Project shadows onto a fixed oriented floor
|
static TrueShadingBuilder.SurfaceOrientType |
TrueShadingBuilder.SurfaceOrientType.NONE
Do not project shadows
|
Modifier and Type | Method and Description |
---|---|
TrueShadingBuilder.SurfaceOrientType |
TrueShadingBuilder.surfaceOrientEnum()
Returns the shadow plane surface orientation enum
License requirements: None. |
static TrueShadingBuilder.SurfaceOrientType |
TrueShadingBuilder.SurfaceOrientType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrueShadingBuilder.SurfaceOrientType |
TrueShadingBuilder.SurfaceOrientType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrueShadingBuilder.SurfaceOrientType[] |
TrueShadingBuilder.SurfaceOrientType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrueShadingBuilder.setSurfaceOrientEnum(TrueShadingBuilder.SurfaceOrientType surfaceOrientEnum)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.