Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType |
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType.HIGH
static image output resolution of 300 DPI (dots per inch)
|
static RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType |
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType.LOW
static image output resolution of 72 DPI (dots per inch)
|
static RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType |
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType.MEDIUM
static image output resolution of 150 DPI (dots per inch)
|
static RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType |
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType.USER_DEFINED
user specified image output resolution in DPI (dots per inch)
|
Modifier and Type | Method and Description |
---|---|
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType |
RayTracedStudioEditorBuilder.rayTracedStudioStaticImageResolution()
Returns the Ray Traced Studio static image resolution
License requirements: None. |
static RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType |
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType |
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType[] |
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RayTracedStudioEditorBuilder.setRayTracedStudioStaticImageResolution(RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType rayTracedStudioStaticImageResolution)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.