Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Method and Description |
---|---|
PointCloudClippingBoxesListItemBuilder |
PointCloudBuilder.createClippingBoxesListItemBuilder()
Creates a
PointCloudClippingBoxesListItemBuilder . |
PointCloudClippingBoxesListItemBuilder |
PointCloudClippingBoxesListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
PointCloudClippingBoxesListItemBuilder[] |
PointCloudClippingBoxesListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PointCloudClippingBoxesListItemBuilderList.append(PointCloudClippingBoxesListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
PointCloudClippingBoxesListItemBuilderList.append(PointCloudClippingBoxesListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PointCloudClippingBoxesListItemBuilderList.erase(PointCloudClippingBoxesListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
PointCloudClippingBoxesListItemBuilderList.erase(PointCloudClippingBoxesListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PointCloudClippingBoxesListItemBuilderList.findIndex(PointCloudClippingBoxesListItemBuilder obj)
Finds the index where the input object appears.
|
void |
PointCloudClippingBoxesListItemBuilderList.insert(int location,
PointCloudClippingBoxesListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
PointCloudClippingBoxesListItemBuilderList.setContents(PointCloudClippingBoxesListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
PointCloudClippingBoxesListItemBuilderList.swap(PointCloudClippingBoxesListItemBuilder object1,
PointCloudClippingBoxesListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.