Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Interface and Description |
---|---|
interface |
IrayPlusMaterialAttributeEnum
Represents a IrayPlus Enum Attribute
This class is restricted to being called from a program running during an Interactive NX session. |
Modifier and Type | Field and Description |
---|---|
IrayPlusMaterialAttribute |
IrayPlusMaterialEditorBuilder.ComponentInfoData.attribueobject |
Modifier and Type | Method and Description |
---|---|
IrayPlusMaterialAttribute |
IrayPlusMaterialEditorBuilder.getComponentParameter(String attribueName)
Gets single attribute object for specific fomatted attribute name
The string attribute name format should be :
"layer name-interface name-attribute name"
Let material ''Varnished Cherry' for example:
If user wants to get 'Base' component's attribueObject of 'Base-Colour-Colour'.
|
Modifier and Type | Method and Description |
---|---|
String[] |
IrayPlusMaterialEditorBuilder.setComponentParameter(String attribueName,
IrayPlusMaterialAttribute attribueObject)
Sets attribute object for specific fomatted attribute name
The string attribute name format should be :
"layer name-interface name-attribute name"
Let material ''Varnished Cherry' for example:
If user wants to set 'Base' component's attribueObject of 'Base-Colour-Colour'.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.