Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static ImageBasedLighting.ImageUpVectorTypes |
ImageBasedLighting.ImageUpVectorTypes.ALIGN_WITH_FLOOR_PLANE |
static ImageBasedLighting.ImageUpVectorTypes |
ImageBasedLighting.ImageUpVectorTypes.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
ImageBasedLighting.ImageUpVectorTypes |
ImageBasedLighting.imageUpVectorType()
Returns the image up vector define
License requirements: None. |
static ImageBasedLighting.ImageUpVectorTypes |
ImageBasedLighting.ImageUpVectorTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ImageBasedLighting.ImageUpVectorTypes |
ImageBasedLighting.ImageUpVectorTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ImageBasedLighting.ImageUpVectorTypes[] |
ImageBasedLighting.ImageUpVectorTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ImageBasedLighting.setImageUpVectorType(ImageBasedLighting.ImageUpVectorTypes imageUpVector)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.